Technical FAQs

Ask a Question

What is the correct method for selecting thermal units for a class 8630 wye delta starter?

Divide the motor full load current by 1.73, and use this quotient to select thermal units from the appropriate tables.


CTA-ID : 2007705
Was this helpful?
What can we do to improve the information ?