Technical FAQs

Ask a Question

Are General Duty switches available in a NEMA 4 enclosure?

No, General Duty switches are only available in NEMA 1 or NEMA 3R enclosures. Consider a Heavy Duty switch for other NEMA 4, NEMA 4X, NEMA 5, NEMA 7, NEMA 9, NEMA 12 or NEMA 12K applications.

CTA-ID : 2007703
Was this helpful?
What can we do to improve the information ?