Technical FAQs

Ask a Question

When is secondary over current protection required on low voltage dry type distribution transformers required?

The proper reference for this is the National Electrical Code (NEC) Table 450.3(b). Table 450-3(b) details the conditions and limits for the over current protection selection for low voltage dry type distribution transfomrers.


CTA-ID : 2007688
Was this helpful?
What can we do to improve the information ?