Technical FAQs

Ask a Question

Customer asks if the contacts on the IEC relays are field convertible?

The contacts are not field convertible on the D-line, K-line, or SK-line relays.


CTA-ID : 2007244
Was this helpful?
What can we do to improve the information ?