Technical FAQs

Ask a Question

GJL thermal magnetic breakers have hold and trip values. Is this adjustable?

No. It is a fixed setting. It will always hold below the hold value. May or may not trip between the hold and trip value. Will always trip above the trip value.

CTA-ID : 2007004
Was this helpful?
What can we do to improve the information ?