Technical FAQs

Ask a Question

Does a QO2TR circuit breaker enclosure have provisions to lock the cover closed with the enclosed circuit breaker handle in either the ON or OFF position?

Issue:
Product Features

Product Line:
Enclosed Molded Case Switch

Cause:
Clarification of standard product features

Resolution:
Yes, the enclosure cover has a padlock provision to allow the cover to be locked closed, regardless of the enclosed circuit breakers handle status.


CTA-ID : 2007675
Was this helpful?
What can we do to improve the information ?