Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a HU362DS, Series F05 or F06, safety switch?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
Ground lugs (2) are provided factory installed. The lugs will each accept (1) #14 - 2 AWG copper conductor or (1) #12 - 2 AWG aluminum conductor.



CTA-ID : 2007670
Was this helpful?
What can we do to improve the information ?