Technical FAQs

Ask a Question

Can you tell me if the QB QD QG QJ breakers are the same size as Q2, and will they fit in the same enclosures, ie, Q22200NS/RB, Q23225NS/RB?

Product features

Product Line:
Circuit Breakers/Enclosures

Clarification of product application

The new QB, QD, QG, QJ circuit breakers fit into the same circuit breaker enclosures as the Q2 circuit breakers did. Dimensionally they are the same.
In a replacement situation, the replacement circuit breaker must have an interrupting rating equal to or greater than that of the circuit breaker originally installed.

CTA-ID : 2007173
Was this helpful?
What can we do to improve the information ?