Technical FAQs

Ask a Question

What is the difference between Forms H10, H20 and H30?

H10 is trip class 10 or quick trip.
H20 is trip class 20 or standard trip.
H30 is user selectable between class 10 or class 20.


CTA-ID : 2001039
Was this helpful?
What can we do to improve the information ?