Technical FAQs

Ask a Question

Can a QON442MS300 load center be either top or bottom fed?

Issue:
Product Design Features

Product Line:
QO load centers

Environment;
Installation of panel 

Cause:
Application

Resolution:
The QON442MS300 is an Obsolete Load center and is no longer available.

The interior was set up for bottom feed as standard. For a top feed application, first rotate the main breaker 180 degrees, then rotate the entire load center interior 180 degrees.

NOTE: When the interior is rotated, the deadfront trim labels will be upside down. The labels should, if handled carefully, may be able to be removed and repositioned for proper orientation.

 
Was this helpful?
What can we do to improve the information ?