Technical FAQs

Ask a Question

Can the EZML332400 Series M03 be supplied with a 250 ampere and a 225 ampere tenant breaker?

Issue:
Current Design Tenant breakers

Product Line:
EZM Metering

Environment:
Series M03 Tenant breakers

Cause:
Different ampere ratings

Resolution:
The EZML332400 current series M03 device comes with a LJL type Circuit Breakers that have an adjustable trip setting ranging from 125 Amp to 400 Amp.  


CTA-ID : 2007429
Was this helpful?
What can we do to improve the information ?