Technical FAQs

Ask a Question

Customer has a HLO1 lockoff. Need something that says the lockoff is UL approved.<br /><br />Call 410-248-3414 direct line

After calling back the HL01 is an unlisted component and does not have a UL mark. If customer wants to research this accessory further, the file number is E10027, Vol 29.


CTA-ID : 2007426
Was this helpful?
What can we do to improve the information ?