Technical FAQs

Ask a Question

Can I add a motor to a P frame breaker if it was not ordered with one?

No. If it was not ordered with a motor, it is impossible to add one. The breaker construction is different.
To replace a motor on a motorized PG PJ or PL breaker, use the kit for the fixed NT.

CTA-ID : 2007423
Was this helpful?
What can we do to improve the information ?