Technical FAQs

Ask a Question

What equipment ground bar is used with a QO120L125GC load center?

Issue:
Product Design Features

Product Line:
QO Load centers

Environment:
Ground bar

Cause:
Application

Resolution:
The PK15GTA ground bar is factory included with this load center, for field installation.


CTA-ID : 2006987
Was this helpful?
What can we do to improve the information ?