Technical FAQs

Ask a Question

Is a filler plate available for a circuit breaker enclosure, to fill the circuit breaker opening in the cover or deadfront trim, in the case the circuit breaker is removed from the enclosure?

Issue:
Is a filler plate available for a circuit breaker enclosure, to fill the circuit breaker opening in the cover or deadfront trim, in the case the circuit breaker is removed from the enclosure?

Product Line:
Circuit breaker enclosures.

Environment:
Product sold in the United States.

Cause:
Availability.

Resolution:
Filler plates are available for enclosures that utilize a QO breaker (QOFP), a Q2 breaker (Q2FP) or a QOM2 breaker (QOM2FP). There are no filler plates for the FA, KA , IK, LA, MA, or NA breakers in their associated enclosures.


CTA-ID : 2007649
Was this helpful?
What can we do to improve the information ?