Technical FAQs

Ask a Question

Are Homeline branch circuit breakers switch duty rated?

Issue:
Product Features

Product Line:
Homeline Circuit Breaker

Cause:
Clarification of product features

Resolution:
Only the 1 pole, 15 and 20 ampere Homeline breakers, HOM115 and HOM120, are switch duty rated.


CTA-ID : 2007645
Was this helpful?
What can we do to improve the information ?