Technical FAQs

Ask a Question

Do the KAL lugs mount via a screw from the bottom into the lug, or from the top into an insert under the terminal?

They mount via a screw from the bottom, through the terminal and into the threaded lug body. When the lugs are removed, the AL250KAIN insert kit must be installed in order to bus mount.

CTA-ID : 2007634
Was this helpful?
What can we do to improve the information ?