Technical FAQs

Ask a Question

Does a QOC342MQS load center cover have the main breaker opening pre-punched?

Issue:
Product Features

Product Line:
QO Load Center Cover

Cause:
Clarification of standard product features

Resolution:
Yes, the main breaker opening in the cover's integral interior trim is pre-punched. If the main breaker load center is converted to a main lugs load center, use filler plate Q2FP to cover the main breaker opening in the cover's integral interior trim.


CTA-ID : 2007413
Was this helpful?
What can we do to improve the information ?