Technical FAQs

Ask a Question

How are trench duct components designated as Aluminum rather than the standard Steel ?

An ``A`` is added to the end of the standard part number and the depth is specified. Aluminum trench duct is available in 2 1/2``, 3`` and 4`` depths.

CTA-ID : 2007204
Was this helpful?
What can we do to improve the information ?