Technical FAQs

Ask a Question

How do you switch from standard duty to heavy duty on the Altistart ATS46?

For heavy duty applications, the controller must be de-rated by one size.

The ATS46 controller is factory preset to standard duty operation. To switch the factory presets to heavy duty applications, remove the control module and change the selector switch to position 2. For the change to take effect, control power must be cycled after adjusting the selector switch.

See ATS46 User`s Manual VD0C32S301B for more details.

CTA-ID : 7462
Was this helpful?
What can we do to improve the information ?