Technical FAQs

Ask a Question

What is the part number for the main lugs mounting keps nut used on HOMELINE MLO load centers?

The keps nut part number is 2342702001. This keps nut connects the lugs to the phase busbars. One is used per phase.

CTA-ID : 2007202
Was this helpful?
What can we do to improve the information ?