Technical FAQs

Ask a Question

What equipment ground bar is used with a HOM24L70RB load center?

Issue:
Product design features

Product Line:
Homeline load centers

Environment:
Ground bar

Cause:
Application

Resolution:
Use PK4GTA. The ground bar is not included. Order separately if an equipment ground bar is required.


CTA-ID : 2006962
Was this helpful?
What can we do to improve the information ?