Technical FAQs

Ask a Question

What is the operating temperature range for the SDM1VC, SDM1VCC, SDM2VC and SDM2VCC video cameras?

The cameras can be used in temperatures ranges of -10 degree C to +50 degree C (+14 degree F to +122 degree F).

CTA-ID : 2006955
Was this helpful?
What can we do to improve the information ?