Technical FAQs

Ask a Question

I need the torque value required to turn the breaker on and off for the LA and LH 3 pole breakers.

Handle force for the LA and LH breakers is 45 lbs. applied 3/8`` from the end of the handle for ON, OFF, and RESET operations.

CTA-ID : 2007400
Was this helpful?
What can we do to improve the information ?