Technical FAQs

Ask a Question

How do you open the padlock slot on the Vario handles?

There is a button with an arrow on the face of operator. With the operator in the off position, push the button to open the padlock slot for use. Be sure that the shaft set screw on the operator is tightened to prevent obstruction of the button from behind.


CTA-ID : 2007190
Was this helpful?
What can we do to improve the information ?