Technical FAQs

Ask a Question

What does the T suffix mean in a HOMELINE load center catalog number?

Issue:
product design features

Product Line:
Homeline load centers

Environment:
Catalog logic

Resolution:
The T indicates that an equipment ground bar is factory installed.


CTA-ID : 2007187
Was this helpful?
What can we do to improve the information ?