Technical FAQs

Ask a Question

What is the Neutral Assembly for a DU323 safety switch?

Issue:
Selection

Product Line:
GD Safety Switch

Cause:
Selection of neutral assembly

Resolution:
The neutral assembly used for the DU323 is dependent upon the Series number of the switch. For Series F1 or F3, use SN0610. For Series E1, or prior designs, a field installable neutral assembly was not available.


CTA-ID : 2007606
Was this helpful?
What can we do to improve the information ?