Technical FAQs

Ask a Question

What does the RB suffix of a safety switch catalog number indicate?

NEMA 3R safety switches with a RB suffix (30 - 200 ampere) in the catalog number will have a hub opening in the top endwall. It will accept 3/4`` through 2 1/2`` B type hubs. The hub opening is covered with a closing cap (BCAP). Hubs are ordered separately. NEMA 3R safety switches with a R suffix (400 - 1200 ampere) do not have a hub opering in the top endwall. A field cut opening is required for top conduit entry. B type hubs, 3`` through 4`` can be used. Hubs are ordered separately.

CTA-ID : 2007382
Was this helpful?
What can we do to improve the information ?