Technical FAQs

Ask a Question

What are the rail and deadfront extensions required to mount an NQOD442L400 or NQOD442L400CU in an MH68 or MH68WP?

The following parts will be required per panel and can only be installed at the mains end:

(1) 80120-823-05 15`` left rail extension
(1) 80120-824-05 15`` right rail extension
(1) 80110-876-05 MLO cover 15`` extension
(4) 21590-17081 Rail extension screws

Revised 3/10/04

CTA-ID : 2007591
Was this helpful?
What can we do to improve the information ?