Technical FAQs

Ask a Question

What is the AL1200P25K4 lug kit data for Powerpact P frame and NS630b - NS1250 breakers?

Conductor: Al/Cu
Lugs per kit: 4
Construction: Individually-mounted breakers.
Tool required: Screwdriver, POZIDRIV #2 or #3, or slotted. Socket Wrench, 7mm hex (for wire binding screw). Torque Wrench, 5/16 in. or 8mm.
Conductors: 4
Size: 3/0 - 500 kcmil
Strip length: Top holes 1.25 in., Bottom holes 2.25 in.
Wire binding screw torque: 442.5 lb-in
Lug mounting screw torque: 190 lb-in


CTA-ID : 2007586
Was this helpful?
What can we do to improve the information ?