Technical FAQs

Ask a Question

What are the termination provisions for SquareD/Schneider Electric`s Sealed Epoxy Resin Encapsulated dry type Transformers (style A, B, and C enclosures)?

Terminations for Sealed Epoxy Resin Encapsulated Transformers

Product Line:
LV Transformers

Applies to Sealed Epoxy Resin Encapsulated Transformers by SquareD/Schneider Electric

Transformer Terminations must be connected to the external circuit

The terminations are conductor leads to which the installer connects the incoming conductors using an appropriate connector of their choice.

CTA-ID : 2007389
Was this helpful?
What can we do to improve the information ?