Technical FAQs

Ask a Question

Are shorting straps available for the D10 disconnect switches?

Yes, select from the following based on switch used:

D10S1 & D10S1H, order D12C01 (includes 3 shorting straps).
D10S2 & D10S2H, order D12D02 (includes 3 shorting straps).
D10S3 & D10S3H, order D12E03 (includes 3 shorting straps).
D10S4 & D10S4H, order D12F04 (includes 3 shorting straps).


CTA-ID : 2004037
Was this helpful?
What can we do to improve the information ?