Technical FAQs

Ask a Question

How many hub closing plates(ACP or ACPL type) are supplied with the Meter-Pak Metering devices?

Issue:
Product Design Features

Product Line:
Meter Pak Metering Equipment

Environment:
Hub provisions

Cause:
Application and installation

Resolution:
It depends on the specific catalog number of the MP device. PLEASE refer to the appropriate 2D CAD Drawing for the specific device catalog number. A link is provided below to access the 2D CAD Drawing page.
http://products.schneider-electric.us/technical-library/?event=search.cad

CTA-ID : 2007109
Was this helpful?
What can we do to improve the information ?