Technical FAQs

Ask a Question

Can the branch connectors only be replaced in a HOMELINE load center?

No, the connector fingers are an integral part of the busbar (one piece construction). The busbars are not individually replaceable, either. A complete interior would be required to replace any portion of the phase or neutral bussing components. The load center catalog number and series number are required to determine the interior part number required.

CTA-ID : 2007147
Was this helpful?
What can we do to improve the information ?