Technical FAQs

Ask a Question

What equipment ground bar is used with a QON42MS400 load center?

Use PK27GTA or PK15GTA6. The ground bar is not included. Order separately if an equipment ground bar is required.


CTA-ID : 2006906
Was this helpful?
What can we do to improve the information ?