Technical FAQs

Ask a Question

What equipment ground bar is used with a QON442MS300 load center?

Issue:
Product design features

Product line:
QO load centers

Environment:
Ground bar

Cause:
Application

Resolution:
The equipment ground bars can be either the PK27GTA or PK15GTA6.  Order the ground bar separately if an equipment ground bar is required.


 
Was this helpful?
What can we do to improve the information ?