Technical FAQs

Ask a Question

What is the CU1200P24K lug kit data for Powerpact M, P frame breakers?

Conductor: Cu
Lugs per kit: 1
Construction: I-LINE M and P frame breakers, Individually-mounted M frame breakers.
Tool required: Screwdriver, POZIDRIV #2 or #3, or slotted. Socket Wrench, 7mm hex (for wire binding screw). Torque Wrench, 5/16 in. or 8mm.
Conductors: 4
Size: 3/0 - 500 kcmil
Strip length: 1.2 in.
Wire binding screw torque: 442.5 lb-in
Lug mounting screw torque: 190 lb-in

CTA-ID : 2007583
Was this helpful?
What can we do to improve the information ?