Technical FAQs

Ask a Question

Is there a line side and a load side to a PXL type breaker?

No, may be fed from either direction. If supplied with ground fault, ensure CT is properly oriented per instructions.

CTA-ID : 2007139
Was this helpful?
What can we do to improve the information ?