Technical FAQs

Ask a Question

What is the difference between the LD4LC030 and the LD4LC130 Integral 32 starters?

The LD4LC030 is the standard in the USA and it has a red handle with a yellow background. However, in Europe, the standard is the LD4LC130 which has a black handle with a blue background. In Europe, the red/yellow handle is reserved for Emergency Stop applications.


CTA-ID : 2007131
Was this helpful?
What can we do to improve the information ?