Technical FAQs

Ask a Question

What equipment ground bar is used with a HOM3040M200TC load center?

Product Design features

Product Line:
Homeline load centers

Ground bars



The PK18GTA ground bar and LK100AN lug were factory installed in this load center. But this load center is Obsolete, no longer available and replaced by the HOM3060M200PC, but the ground bar and larger lug will need to be purchased separately with the new load center. The catalog number of the ground bar is PK23GTA and the larger branch neutral lug is the LK100AN.

CTA-ID : 2007566
Was this helpful?
What can we do to improve the information ?