Technical FAQs

Ask a Question

Does an MCT-12B or MCT-14B clock/timer require a back box? If so, what is the appropriate catalog number?

Issue:
Does an MCT-12B or MCT-14B clock/timer require a back box?  If so, what is the appropriate catalog number?

Product Line:
Medical Products.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
When the MCT-12B is installed in the Surgical Facility Panel, no additional components are required.  When the MCT-12B is to be mounted in a wall, then both a back box (catalog number 53007BB) and a stainless steel trim plate (catalog number MCTS95135) are required.  If utilizing the MCT-CT remote control unit for the MCT-12B, the MCT-CT requires an ordinary 2-gang back box which must be supplied by the installer.

The MCT-14B is only wall mountable and requires a 53006BB back box.  The MCT-14B also requires a MCT-4RC auxiliary control, which itself requires a 53008BB back box.


CTA-ID : 2006667
Was this helpful?
What can we do to improve the information ?