Technical FAQs

Ask a Question

What are the part numbers for the replacement ring nut, locking thrust washer, trim washer, and rubber sealing washer for the 9001 J pilot lights?

Ring nut is 6512909601, locking thrust washer is 6512909201, trim washer is 6512909301, and the rubber sealing washer is 6512909801.


CTA-ID : 2007126
Was this helpful?
What can we do to improve the information ?