Technical FAQs

Ask a Question

What contacts are available for the operator mounted in the base or bottom of a standard XACA pendant station?

XACS101 is one normally open contact
XACS102 is one normally closed contact
XACS103 is two normally open contacts
XACS104 is two normally closed contacts
XACS105 is one normally open and one normally closed contact.


CTA-ID : 2007124
Was this helpful?
What can we do to improve the information ?