Technical FAQs

Ask a Question

What equipment ground bar is used with a QO140M200 load center?

Issue:
Product Design Features

Product Line:
QO Load centers

Environment:
Ground bar

Cause:
Application

Resolution:
Use PK23GTA. The ground bar is not included. Order separately if an equipment ground bar is required.


CTA-ID : 2007340
Was this helpful?
What can we do to improve the information ?