Technical FAQs

Ask a Question

Are any of the MP Meter-Pak Devices available with more than six tenant breakers or meter sockets?

Product Design

Product Line:
MP Meter Pak Metering

Quantity of Meter sockets

Additional tenants


No, the MP Meter-Pak Meter Centers are only available with a maximum of up to six meter sockets and tenant breakers, to comply with the NEC(National Electrical Code). Basically, the NEC states that when more than six disconnects are supplied, an overall main disconnect must be used and the MP Meter Pak devices are NOT designed with a overall Main Disconnect. For applications requiring more than 6 meter sockets and tenant breakers, consider using the EZM Metering products.

CTA-ID : 2007118
Was this helpful?
What can we do to improve the information ?