Technical FAQs

Ask a Question

Can a 100A HCN panel with a vertically mounted ``FA`` main be converted from bottom to top feed?


1. Rotate entire panel assembly 180 degrees.

2. Replace factory installed main breaker with a top-feed breaker. (Example: FA36100MT)

3. In some cases, the main breaker cover plate (part of interior deadfront) must also be rotated 180 degrees to achieve proper orientation of deadfront labels.

CTA-ID : 2007764
Was this helpful?
What can we do to improve the information ?