Technical FAQs

Ask a Question

Can I interlock 3 MAL36800 breakers together?

No, only two with the walking beam system. But you can interlock three with the NW fixed or drawout breakers. Use the following interlock kits:
Three main circuit breakers: S48610
Two main circuit breakers and one tie: S48609
Two main circuit breakers and one generator breaker: S48608


CTA-ID : 2007759
Was this helpful?
What can we do to improve the information ?