Technical FAQs

Ask a Question

Is the cylinder on a 9025GXW2 threaded<br />541-667-2070

It is not threaded. Have to secure by another mechanical means. See the Help Files for additional information on installation of these devices, currently in book 112.


CTA-ID : 2007538
Was this helpful?
What can we do to improve the information ?