Technical FAQs

Ask a Question

When installing a SDSA3650, what practices should the installer consider regarding the lead conductors?

Confirm that the terminals used to terminate the lead conductors are suitable for the conductor size (#12 AWG stranded wire). Twist the conductors 1/2 turn or more for every twelve inches of length. Keep the conductor length as short as possible with no sharp bends. Do not loop or coil the conductors.

CTA-ID : 2007529
Was this helpful?
What can we do to improve the information ?