Technical FAQs

Ask a Question

What is the Solid Neutral Assembly for a DU324RB General Duty Safety Switch?

Issue:
Selection

Product Line:
General Duty Safety Switch

Environment:
Accessories

Cause:
Selection

Resolution:
The neutral assembly used for the DU324RB is dependent upon the Series number of the switch. For Series F1(or F01), use the SN20A. For Series E2 or E3, use SN225KA. For Series E1, or prior designs, a field installable neutral assembly was not available.

 
Was this helpful?
What can we do to improve the information ?